Hello everyone,
I am new to yocyo/fsl, but I have been struggling with something off-and-on all week. I have a target image for imx53evk that includes everything that I can figure is related to building applications so that I can build on the target. Most everything is getting included on the target image, but the GStreamer package (package definition, headers, etc.) and the libs/headers for the IPU and VPU APIs are missing. The are in the sysroot build/tmp/sysroots/imx51evk, but they don't appear in the target image. I've tried everything I can think of, and scoured the web looking for a clue, but I'm at a loss.
Many thanks,
--mark
Hi Mark
had you looked at i.MX53 QSB links
L2.6.35_11_09_ER_SOURCE : Linux 2.6.35 Source Code Files and documentation 11.09.
Supports MCIMX53-START and MCIMX53-START-R.
IMX53_11_09_LINUX_MMCODECS : "Linux Multimedia Codecs Documentation and
Sources 11.09 for i.MX53 for the Quick Start boards
Note, community yocto releases may lack some proprietary FSL multimedia packages,
differencies are described in
https://community.freescale.com/message/402940#402940
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------