i.MX6 Ethernet Compliance Testing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Ethernet Compliance Testing

1,211 Views
kevinharvey
Contributor I

Hello all,

I'm attempting to do some ethernet compliance testing on a Phytec Phyflex i.MX6D SoM.  The compliance software provided by Keysight/Agilent requires the device being tested to transmit scrambled, 3-level random bit sequences to capture the waveforms it needs.  Is there an application available that will accomplish this?  I know some platforms have ethernet utilities that allow the device to enter certain test modes but I'm not having much luck finding anything like that in this case.

Thanks for any help you can provide!

Kevin

Labels (3)
0 Kudos
1 Reply

528 Views
Yuri
NXP Employee
NXP Employee

  Please note that test pattern for i.MX6 Ethernet Compliance Test is applicable to Phy.

Since i.MX6 has not Ethernet Phy, so this is not applicable to i.MX6.

Please apply to Phy vendor which is used on custom board for Ethernet Compliance

Test data.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos