AnsweredAssumed Answered

Corrupted BSC9132 QorIQ Qonverge Flash?

Question asked by Robert Steadman on May 7, 2015
Latest reply on May 8, 2015 by Robert Steadman

Hi,

When I boot our BSC9132 QorIQ Qonverge development board the following output is displayed (via the attached serial link):

NAND boot... WARNING: ECC not checked in SPL, check board cfg

 

U-Boot 2011.06.WUSDK_1.1-00008-g35c3242 (Jul 23 2012 - 13:18:42)

 

CPU0:  BSC9132E, Version: 1.1, (0x86180011)

Core:  E500, Version: 5.2, (0x80211152)

Clock Configuration:

       CPU0:1200 MHz, CPU1:1200 MHz,

       CCB:600  MHz,

       DDR:800  MHz (800 MT/s data rate) (Asynchronous), IFC:150  MHz

L1:    D-cache 32 kB enabled

       I-cache 32 kB enabled

Board: BSC9132QDS

Sys ID: 0x1f, Sys Ver: 0x31, FPGA Ver: 0x78,

IFC chip select:NAND

I2C:   ready

SPI:   ready

DRAM:  880 MiB (DDR3, 32-bit, CL=6, ECC off)

Flash: *** failed ***

### ERROR ### Please RESET the board ###

 

I assume that the flash memory has been corrupted, but I don't know quite how to confirm that and fix it.

I have seen what I think is s similar problem, on a different board, in another thread where CodeWarrior and a USB TAP were used to reprogram the board. We have similar equipment.

Is anyone able to advise?

 

Thanks,

 

Robert

Outcomes