AnsweredAssumed Answered

Problem with "git clone" on git.freescale.com

Question asked by Christian Treczoks on May 6, 2015
Latest reply on Jan 11, 2016 by Saurabh Patel

Hi!

 

I'm trying to set up an android 4.4 for a board based on the sabre design. I got the documentation and try to follow it to the point, but I'v come across a problem:

 

When I try to "git clone git://git.freescale.com/imx/linux-2.6-imx.git kernel_imx" I get a

Cloning into 'kernel_imx'...

fatal: unable to connect to git.freescale.com:

git.freescale.com[0: 192.88.156.202]: errno=Connection refused

 

I can ping the machine, and I can access it from the browser.

 

Then I tried "git clone http://git.freescale.com/imx/linux-2.6-imx.git kernel_imx" to go through port 80 instead (which is open), but then I got:

Cloning into 'kernel_imx'...

fatal: http://git.freescale.com/imx/linux-2.6-imx.git/info/refs not found: did you run git update-server-info on the server?

 

Any ideas? I've to admit that I'm rather clueless about git...

 

Yours, Christian

Outcomes