AnsweredAssumed Answered

Video doesn't play on repeated playback

Question asked by Ramakrishna kamath on May 4, 2015

Video property is as follows :

 

Topology:

container: Quicktime

audio: MPEG-4 AAC

video: H.264

 

Properties:

Duration: 0:15:20.810000000

Seekable: yes

Tags:

video codec: H.264 / AVC

maximum bitrate: 3695752

bitrate: 749856

audio codec: MPEG-4 AAC audio

language code: en

datetime: "2013-07-05T14:54:42.000000+0530"

container format: ISO MP4/M4A

 

Our pipeline

gst-launch-0.10 filesrc location=/mnt/usb/301869/L2.0_320_176.mp4  typefind=true ! aiurdemux name=demux demux.video_000000 ! queue ! vpudec ! mfw_v4lsink demux.audio_000000 ! queue ! aacparse ! beepdec ! alsasink -v

 

Attached gst_debug log of Vpudec.

 

It is not reproducing always. On repeated playback we observed sometimes.

If we enable gstreamer debug log, we are able to reproduce always.

 

We are using gst-fsl-plugins version 3.5.7 and gstreamer version 10.36

 

Result of "uname -a" is

Linux freescale 3.0.35-2154-g94689e1 #180 SMP PREEMPT Wed Mar 4 15:24:49

CST 2015 armv7l GNU/Linux

 

BSP version is 3.0.35 based customized BSP.

Board is IM6D based customized board .

 

This is very urgent, for a production program. SOP is very close.

Please help us analysing this ASAP.

 

Thanks and Regards:

Ramakrishna Kamath

Original Attachment has been moved to: vpudec_failure.txt.zip

Outcomes