Can a non-Mipi cmos image sensor (CMOSIS CMV4000) be interfaced to i.MX6 CSI ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can a non-Mipi cmos image sensor (CMOSIS CMV4000) be interfaced to i.MX6 CSI ?

543 Views
ellerre
Contributor I

The sensor delivers 12 bit row data through 2(4) lvds DDR lanes + differential clock but data sheet doesn't state it is Mipi compliant.

Additional frame sync and pixel valid signals are available and could be input to IPE VSYNC and HSYNC.

Can serial stream (not parallel) be captured this way?

Nuova immagine bitmap.bmp

Labels (1)
0 Kudos
1 Reply

324 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I.MX6 has camera input with serial input (MIPI-CSI-2) however it does not support LVDS input.

Best Regards,

Alejandro

0 Kudos