SPI MQX set delays

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI MQX set delays

Jump to solution
623 Views
cwati
Contributor III

Hi there,

I've been trying to port some SPI code from basic KSDK 1.0.0 to MQX 4.1 (SPI not SPI legacy).

Code works smoothly in KSDK 1.0.0, but I notice some timing issues in MQX 4.1.

We use the following set delays in KSDK.  Is there similar set delay functionality in MQX for SPI?

  status = DSPI_DRV_MasterSetDelay(instance,

    kDspiPcsToSck,

    500, // delayInNanoSec

    & calculatedPcsToSck);

  if (status != kStatus_DSPI_Success)

  return false;

    status = DSPI_DRV_MasterSetDelay(instance,

    kDspiLastSckToPcs,

    500, // delayInNanoSec

    & calculatedLastSckToPcs);

  if (status != kStatus_DSPI_Success)

  return false;

  status = DSPI_DRV_MasterSetDelay(instance,

    kDspiAfterTransfer,

    500, // delayInNanoSec

    & calculatedAfterTransfer);

  if (status != kStatus_DSPI_Success)

  return false;

Thanks,
Cecylia

Tags (4)
0 Kudos
1 Solution
363 Views
cwati
Contributor III

Hmmmpf, doesn't seem like MQX has explicit IOCTLs to set delays (KSDK "DSPI_DRV_MasterSetDelay") but if you set the baud rate correctly, MQX' "_dspi_find_baudrate" will resolve it for you.

View solution in original post

0 Kudos
2 Replies
364 Views
cwati
Contributor III

Hmmmpf, doesn't seem like MQX has explicit IOCTLs to set delays (KSDK "DSPI_DRV_MasterSetDelay") but if you set the baud rate correctly, MQX' "_dspi_find_baudrate" will resolve it for you.

0 Kudos
363 Views
danielchen
NXP TechSupport
NXP TechSupport

I think in mqx, you can use wait function, but the resolution is not fine. Thank you for your sharing.

0 Kudos