SR: 1-3758282791
Our customer is triing to boot Windows Embedded Compact 7 from MT29F2G08ABBEAH4:E Micron NAND flash on i.MX51 board
They have follow the pdf AN3986, Changing the i.MX51 NAND Flash Model for Windows Embedded CE TM 6.0 and i am using the BSP version WCE700_11.06.01_ER.
They added the MT29F2G08.inc file and MT29F2G08.h in following path:
C:\WINCE700\platform\common\src\soc\COMMON_FSL_V3\NAND\INC
As the pdf AN3986 mentioned they have created the environment variable BSP_NAND_ MT29F2G08.
They selected the catlog item under storage device /MSflash drivers/ Flash MDD and rebuilt the OS image.
Then they are getting this using Mfgtools-Rel-1.6.2.0322 to burn eboot.nb0 and nk.nb0 files:
Windows CE Kernel for ARM (Thumb Enabled) Built on Aug 4 2010 at 14:23:58
INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0xb
OEMInit: silicon r
Ù= 0x20
BoardID = 0x0.
OALIoCtlHalInitRTC(2006/1/1 12:0:0.000)
OTG : Load HCD
OTG : Unload HCD
OTG : Load UFN
BOT_InternalInit with Drivers\Active\15
Exception 'Data Abort' (4): Thread-Id=015a0006(pth=832402f4), Proc-
Id=00400002(p
prc=80589308) 'NK.EXE', VM-active=017f0002(pprc=9662db40)
'udevice.exe'
PC=c0153860(gwes.dll+0x00053860)
RA=c0153848(gwes.dll+0x00053848) SP=d079fdd8, B
VA=00000104
UFN_ATTACH with key = Drivers\Active\15
UFN_CONFIGURED: BOT_OpenInterface again
UTP command:Media type: NAND.
UTP command:QueryStoreStatus.
UTP command:Check if disk is ready.
Please be patient to wait...
Send storage disk name: DSK1:.
Send time out: 10.
Opening disk DSK1: failed.Error code is 4319
Opening disk DSK1: failed.Error code is 4319
Opening disk DSK1: failed.Error code is 4319
Deactivated user can you help to review this case?