Can i.MX6 MIPI-CSI capture YUV400 and YUV444?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i.MX6 MIPI-CSI capture YUV400 and YUV444?

Jump to solution
874 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6 MIPI-CSI.

Please see chapter 41.2 in IMX6SDLRM Rev.1, it says these formats are supported.

RGB, YUV and RAW color space definitions

From 24-bit down to 6-bit per pixel

According to this description, YUV400 (14-bit) and YUV444 (24-bit) are supported.

However, these format is not mentioned in chapter 41.5.x.

So I want to confirm whether i.MX6 MIPI-CSI can capture YUV400 and YUV444.

Would you let me know it?

Best Regards,

Satoshi Shimoda

Labels (4)
Tags (2)
0 Kudos
1 Solution
615 Views
SergioSolis
NXP Employee
NXP Employee

Hello Satoshi,

It is supported but it is not implemented. You would need to implement by on your side.

View solution in original post

0 Kudos
1 Reply
616 Views
SergioSolis
NXP Employee
NXP Employee

Hello Satoshi,

It is supported but it is not implemented. You would need to implement by on your side.

0 Kudos