Hi,
I am trying to put KL05 to VLLS1 mode. I have configured LLW_P6 /PTB4 to wake up in falling edge.
My problem is, the microcontroller is going to VLLS1 mode. But It is not waking up when I change the state of LLW_P6/PTB4 to low.
/************************************************************ This is my code *************************************************************************/
#include "derivative.h" /* include peripheral declarations */
#include "SpiComm.h"
#include "dma.h"
#include "timer.h"
#include "globals.h"
#define SET_NMI_INTERRUPT() SCB_ICSR |= SCB_ICSR_NMIPENDSET_MASK
#define PORTB_TOGGLE(n) GPIOB_PTOR = 0x0001 << (n)
#define PORTB_SET(n) GPIOB_PSOR = 0x0001 << (n)
#define PORTB_CLR(n) GPIOB_PCOR = 0x0001 << (n)
#define PORTB(n) GPIOB_PDIR & (0x01 << (n))
void InitPortB(){
SIM_BASE_PTR->SCGC5 |= 0x01 << 10; // Enable clock
PTB_BASE_PTR ->PDDR |= 0x01 << 8; // Direction : Output
PTB_BASE_PTR->PDOR = 0x01; // Initial value = 0
PORTB_BASE_PTR->PCR[8] = 0x01 << 8; // Enable MUX
PTB_BASE_PTR->PDDR &= ~(0x01 << 4); // PTB4 as input
PORTB_BASE_PTR->PCR[4] |= 0x01 << 8; // Enable MUX for PTB4
PORTB_BASE_PTR->PCR[4] |= 0x01 << 1; // Enable Pull-up/Pull-down
PORTB_BASE_PTR->PCR[4] |= 0x01 << 0; // Enable Pull-up resistor
// PORTB_BASE_PTR->PCR[4] |= 0x08 << 16; // Interrupt when logic '1'
// NVIC_BASE_PTR->ISER |= (uint32_t)(0x01 << 31);
}
void InitPortA(){
GPIOA_PDDR &= ~(0x1000);
PORTA_PCR12 &= ~(0x01 << 8);
PORTA_PCR12 |= 0x01 << 8;
PORTA_PCR12 |= 0xB0000;
((NVIC_MemMapPtr)0xE000E100)->ISER |=0x01<<30;
}
void Set_VLLS1(){
uint8_t temp1 = 0;
// Configure VLLS Mode
SMC_PMPROT = 0x02; // Allow Low Leakage Power Modes (VLPR,VLPW,VLPS,LLS)
temp1 = SMC_PMPROT; // Dummy read
SMC_PMCTRL = 0x04; // Run and Stop Mode Control (RUN,VLPR,VLPS,LLS,VLLSx)
temp1 = SMC_PMCTRL; // Dummy read
SMC_STOPCTRL = 0x01; // Select VLLS1
// Configure Wakeup source
LLWU_PE2 = 0x20; // Enable LLW_P6/PTB4 as wakeup source (Falling edge)
LLWU_ME = 0x40; // Enable LLWU Module 6
LLWU_F1 |= 0x01 << 6;
LLWU_F3 |= 0x01 << 6;
}
int main(void)
{
unsigned int count1 = 0x00;
InitPortB();
TimerInit();
SPI_Init(); //
Set_VLLS1(); // Configure sleep mode
PORTB_SET(8);
for(count1=0; count1<128; count1++){
SpiBuff[count1] = 0x0A + count1;
}
while(1){
if(TimeCount == 500){ // If count reached
TimeCount = 0; // Clear count
SCB_SCR|=SCB_SCR_SLEEPDEEP_MASK; // Enable ARM deep sleep modes
__asm("WFI"); // Go to sleep
}
if(PORTB(4)){
asm("nop");
}
}
return 0;
}
Did I miss something or did I do something wrong??
Please help me guys..
Thanks and regards
Varun Rajarangan
Hi Varun Rajarangan,
Yes, you are right, NVIC won't run in VLLS1, so actually the LLWU interrupt is executed after wakeup reset.
Wish it helps you!
Have a great day,
Jingjing
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------