Can we use Kinetis Software Development Kit (KSDK) For TWR – K20D72M BOARDS . Is there any document for creating MQX project with KDS for – K20D72M BOARDS
Hi ,
The current KSDK and next released version have not supported TWR-K20D72M yet, so if you want to develop an application based on that, I would recommend MQX 4.1 which already supports TWR-K20D72M, and it supports KDS as well, so you needn't start from scratch, you may use some example as a starting point. Please kindly refer to Freescale MQX™ Software Solutions|Freescale for more details.
Hope that helps,
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I have downloaded MQX 4.0 can I use it on KDS for TWR-K20D72M , or should I download MQX 4.1 for this purpose? Can u specify the exact version and link for download.
MQX 4.1 is the latest version, so I recommend 4.1, but 4.2 is on the way now, and I was told 4.2 would be available by the end of April. anyway, you may get the latest version by the following link:
Freescale MQX™ Software Solutions|Freescale
Hope that helps,
Best Regards,
Kan
Hello,
As Kan mentions, MQX_4.1.1 has KDS support. I have used it and run code on TWR-K20D72M tower hardware.
I even used the KDS to add processor expert support to the K20D72M BSP and got it to work.
Regards,
David
can any one share the steps to create MQX project for TWR_K20D72M board using KDS_2.0.0,KSDK_1.1.0 and MQX 4.1 should i install any thing else , i was using opensource JTAG in codewarrior what all should be done to use source JTAG in KDS .
I haven’t seen the option to create MQX project for TWR_K20D72M board , I have seen the same processor option in KDS , is the TWR_K20D72M board platform actually available in KDS .
Can u give a detailed reply ?
Hello joseph,
Unfortunatelly in KSDK 1.1 neither KSDK 1.2. (the newest version) there is no support for TWR_K20D72M.
So you can create new project in KDS 3.0 but not with KSDK.
You can check the information at Release Note for KSDK here http://cache.freescale.com/files/soft_dev_tools/doc/support_info/KSDK120RN.pdf?fpsp=1&WT_TYPE=Suppor...
So I recommend you work with new MQX 4.2, there is support for your board.
You can check it with Release Note for MQX 4.2. http://cache.freescale.com/files/soft_dev_tools/doc/support_info/MQX_Release_Notes.pdf?fpsp=1&WT_TYP...
For installation MQX 4.2:
and that´s it.
For next steps I recommend follow documentation and follow created examples.
For the
For installation KDS 3.0, please go to Kinetis Design Studio Integrated Development |Freescale
New Kinetis Design Studio V3.0.0 available
In case of other questions, contact us.
I hope this helps you,
Best Regards,
Iva