Hi,
Can anyone tell me where to download MIMP (Motorola Impedance Matching Program)? I'll appreciate it.
Btw, I downloaded it through Google, but it cannot be installed in 64-bit Windows 7 system.
thanks.
Ben
Hi Ben,
The MIMP was in distribution as Motorola's DK107/D 5.25" flopy disk, now it is not available from Freescale anymore. Program was developed in 1993 or earlier, so it is DOS version only, not supported by Windows.
Please try to run this program under some DOS emulator, it should work.
Best regards,
Wlodek_D.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
it does work.Highly appreciate your kind help.Ben