Product: CodeWarrior for MCU
Version: 10.6
Build Id:140329
Target Board: TWR-S08DC-PT60
Reproducible Steps:
After using the board (stand-alone) in debug mode, I then tried to program the code using the flash programmer.
After this, I can no longer connect to the target board.
The windows Device Manager does show: PEMicro USB Serial Port (i1)
I can't see any other related device or enumerated Com port under device manager (should I ?)
Could my code have locked out the on board BDM?
The code did a simple led flash, which worked fine under debug.
Attached are the diagnostic files...
regards
Russell
Original Attachment has been moved to: 201504232219_WorkspaceLog.txt.zip
Original Attachment has been moved to: 201504232219_ConfigurationDetails.txt.zip
Original Attachment has been moved to: EventDetails.txt.zip
Hi
Do you still have problems?