AnsweredAssumed Answered

i.MX6SDL IPU CSI capability when use both parallel camera port and MIPI-CSI2.

Question asked by Satoshi Shimoda on Apr 23, 2015
Latest reply on Apr 29, 2015 by Yuri Muhin

Hi community,

 

We have a question about i.MX6SDL IPU CSI capability.

Please see page 2790, 2791 in IMX6SDLRM Rev.1.

There are the CSI capability to input via parallel port or MIPI-CSI2 individually.

Then, how about when use both port (parallel and MIPI-CSI2)?

 

For example, how judge whether i.MX6SDL can receive the following input?

 

Parallel: 1920 x 1080 x 30fps x 1.35 x 2(YUV422 over 8 bit) = 168MHz

MIPI-CSI2: 1280 x 1024 x 30fps x 1.35 x 1.5(RGB888) = 89MHz (1.9Gbps)

 

 

Best Regards,

Satoshi Shimoda

Outcomes