I set up KDS 2.0 and I am looking for sample applications for the TWR-K22F120M Board.
I cannot find them anywhere. Also I do not see this board option when I try and create a new project.
Can anyone help me with this?
Hello Joseph,
After you install the KSDK on KDS, when you create project , you will find the option of "TWR-K22f120m"
Now the latest Ksdk version is KSDK1.1.0 , please download here : Software Development Kit for Kinetis MCUs|Freescale
Please refer to here for install and update the KSDK : ...Freescale\KDS_2.0.0\KDS200RN.pdf -> 4 Using Kinetis Design Studio with the Kinetis SDK .
(About install and Eclipse update , you can also refer to the attachment )
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Joseph
If you don't find anything suitable in the existing packages you can still fall-back on a complete and supported solution at http://www.utasker.com/kinetis/TWR-K22F120M.html
which works out-of-the box with
If you are using the board for hobby or educational work all tools and resources are completely free and supported in this forum. If you have a commercial use it includes personal support so that you lose no project time.
Regards
Mark
Kinetis: µTasker Kinetis support
K22: µTasker Kinetis FRDM-K22F support / µTasker Kinetis TWR-K22F120M support
For the complete "out-of-the-box" Kinetis experience and faster time to market