AnsweredAssumed Answered

How to create a set MQX libs of  for a custom board in CW 10.6/MQX 4.1.1

Question asked by James McNamara on Apr 9, 2015
Latest reply on Apr 15, 2015 by Radek Sestak

I am trying to update a completed project built with MQX 4.0 and CW 10.4 to the latest CW 10.6 and MQX 4.1.1. To start with, I imported the example twrk60n512 MQX library projects as I have always done with CW 10.4. But building them did not generate code. So I tried copy and paste of the .WSD file into the project window and it caused all the library projects to be imported and then they ran.

 

I have always created MQX library projects for my custom hardware by manually editing the XML .project and .cproject files. But now there is a .WSD file, which is an XML file as well. But the .WSD files have no line separators, not linux or windows format. So editing those will be a real pain.

 

How are we supposed to create new MQX lib projects in the wonderful new world of CW 10.6?

 

Thanks

Outcomes