AnsweredAssumed Answered

Download .sdcard image for i.MX6sx SabreSDB using MFGTool

Question asked by JAVIER VILLAFANA on Apr 8, 2015
Latest reply on Jun 19, 2015 by M T

I followed the Yocto Training up until Task #4 - Deploy and test.... and I got stuck here.

I am not able to download the .sdcard image to my SD card. Do I need to format it first? It is brand new.

Since the sudo dd if=core-image-base-imx6solosabresd.sdcard of=/dev/sdb1 bs=1M did not work for me, I was not able to boot from the SD on my board. The board switches are set to boot from SD4. Is imx6solosabresd the correct MACHINE to use for the solox? I tried setting MACHINE=imx6sxsabersd in the local.conf file but I got an error message (Task #2).

 

This is why I want to try the MFGTool. I have set the board to boot from SD3 so it can go into "download mode". When I go through the MFGTool, it says No Device Connected although HID-compliant vendor-defined device shows up.

Outcomes