AnsweredAssumed Answered

Error in building "libav" and "ffmpeg"

Question asked by Manjunath Joshi on Apr 3, 2015
Latest reply on Apr 9, 2015 by Manjunath Joshi

Hello All,

 

I added packages "libav" and "ffmpeg" in sources/recipies-fsl/images/fsl-image-multimedia.bb but i got the logs as seen below. multimedia images doesn't support this kind of audio/video codec or vice versa. But the same error was found for core-image-minimal as well. Can anyone help me in this?

 

######################################################################################################################################################################################################################################

manju@manju-ThinkCentre-A85:~/projects/yocto/fsl-community-bsp/build$ bitbake fsl-image-multimedia

Loading cache: 100% |###########################################| ETA:  00:00:00

Loaded 2078 entries from dependency cache.

Parsing recipes: 100% |#########################################| Time: 00:00:00

Parsing of 1621 .bb files complete (1619 cached, 2 parsed). 2077 targets, 127 skipped, 0 masked, 0 errors.

NOTE: Resolving any missing task queue dependencies

ERROR: Nothing RPROVIDES 'libav' (but /home/manju/projects/yocto/fsl-community-bsp/sources/meta-pga/recipes-fsl/images/fsl-image-multimedia.bb RDEPENDS on or otherwise requires it)

ERROR: libav was skipped: because it has a restricted license not whitelisted in LICENSE_FLAGS_WHITELIST

ERROR: libav was skipped: because it has a restricted license not whitelisted in LICENSE_FLAGS_WHITELIST

NOTE: Runtime target 'libav' is unbuildable, removing...

Missing or unbuildable dependency chain was: ['libav']

ERROR: Required build target 'fsl-image-multimedia' has no buildable providers.

Missing or unbuildable dependency chain was: ['fsl-image-multimedia', 'libav']

 

Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

#######################################################################################################################################################################################################################################

Which image is most suited for libav or ffmpeg?

 

Regards,

Manju

Outcomes