i.MX6Sololite EVK Board Cannot Install Apps

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Sololite EVK Board Cannot Install Apps

524 Views
nicholassaulnie
Contributor II

Hello All,

The Android 4.0.4 image that comes packaged with the EVK board can install APK files from the internet as long as I enable "unknown sources" under security settings and "usb debugging" under developer options.

I built a version of Android 4.0.4 loosely following the instructions in file 13.5.0_Android_User_Guide from IMX6_R13.5_ANDROID_DOCS_BUNDLE. The built Android seems to work; however, whenever I try to install a downloaded APK file it fails with on-screen message "Application not installed". No serial output is generated when the application fails to install.

Can anyone help me debug and fix this issue?

Thank you,

Nick

Labels (3)
0 Kudos
2 Replies

424 Views
nicholassaulnie
Contributor II

Is it possible that the system would generate an error when it failed to install the app? If so, where would I look to see this error?

0 Kudos

424 Views
SergioSolis
NXP Employee
NXP Employee

Hello Nicholas,

Are you using ADB to install the APK?

0 Kudos