Question about I.Mx6DL Spec sheet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about I.Mx6DL Spec sheet

313 Views
inhojeon
Contributor III

Hi, All


I have a question about I.Mx6 DL Spec sheet of "Table 100" (Below linked spec sheet) 

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLAEC.pdf

What is meaning about  "Value" of Table100 ?

I think it seems like initial state of pins but i wondering about "PU 100K or PD 100K". Is it internal PU or PD?

Please reply this question.

Best Regards,

Inho Jeon.

Labels (1)
1 Reply

285 Views
igorpadykov
NXP Employee
NXP Employee

Hi Inho

you are right: this internal pull resistors value.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------