Using iMX6 Solo and DDR3 - are both diff clock pairs DRAM_SDCLK_0 and DRAM_SDCLK_1 active in the Solo part?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using iMX6 Solo and DDR3 - are both diff clock pairs DRAM_SDCLK_0 and DRAM_SDCLK_1 active in the Solo part?

600 Views
psayles
Contributor I

Using iMX6 Solo and DDR3 - are both diff clock pairs DRAM_SDCLK_0 and DRAM_SDCLK_1 active in the Solo part?

Labels (3)
0 Kudos
1 Reply

358 Views
Yuri
NXP Employee
NXP Employee

Generally signals CS0, ODT0, SDCKE0 relate to the CS0 channel ; signals CS1,

ODT1, SDCKE1 relate to the CS1 channel.

Clock signals SDCLK0 and SDCLK1 in default state are the same and can be used

for both CS0 or CS1 channels if this makes easier PCB design.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos