imx6q-pcie 1ffc000.pcie: phy link never came up on Solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q-pcie 1ffc000.pcie: phy link never came up on Solo

1,193 Views
bonton
Contributor I

Hi

Linux version imx_3.10.53_1.1.0_ga.

I am testing 2 platform Quad and Solo.

They share same design and only the i.MX6 is changed.

While the PCI works fine in the Quad it is not working on the Solo.

dmesg | grep -i pci

imx6q-pcie 1ffc000.pcie: phy link never came up

imx6q-pcie 1ffc000.pcie: failed to initialize host

PCI: CLS 0 bytes, default 64

ehci-pci: EHCI PCI platform driver

Same design with release imx_3.0.35_4.1.0 works fine both Solo and Quad.

Thanks on advance, Bon.

Labels (1)
0 Kudos
2 Replies

613 Views
ivannikolaenko
Contributor IV

Hi Bon Ton!

Did the new BSP solve your issue? I have the same issue with Linux version imx_3.10.53_1.1.0_ga and imx_3.14.28_1.0.0_ga

Best regards, Ivan.

0 Kudos

613 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bon

one can try new Linux BSP

L3.14.28_1.0.0_iMX6QDLS_BUNDLE : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo

Linux Binary Demo Files and Linux BSP Documentation 

Size (K): 1479000 Format: gz Rev #: L3.14.28_1.0.0 Modified: 4/10/2015


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos