Problem : Not booting SABRE BD (I.MX6 Dual Lite) on connecting HDMI to Monitor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem : Not booting SABRE BD (I.MX6 Dual Lite) on connecting HDMI to Monitor

463 Views
inhojeon
Contributor III

Hi all,

First I.MX6 Dual lite SABRE BD(Automotive : Base and CPU Bd) connected monitor on HDMI.

And then, Connect DC Power.

It is not boot.(Just SD boot; attached SD memory card)


But Do not connected monitor on HDMI, And then, connect DC; it is boot.


Inform me about this problems.


best regards,


Inho Jeon

Labels (1)
Tags (1)
0 Kudos
1 Reply

317 Views
igorpadykov
NXP Employee
NXP Employee

Hi Inho

seems this is bug 6703 as described below

HDMI connection causes crash on i.MX6 Solo

https://bugzilla.yoctoproject.org/show_bug.cgi?id=6703

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos