Tony Papadimitriou

ASM8 & ASM11 v9.62 cross assemblers (Win/Linux) are available for download

Discussion created by Tony Papadimitriou on Sep 19, 2009
Branched from an earlier discussion

Latest ASM8 & ASM11 (v9.62) assemblers for Windows & Linux are now available for download (click on the respective page's title to download binaries)

 

In this version:

 

* Some bug fixes (and a long-standing one regarding assumed #include relative path location in Linux version)

* New command-line options

* Ability to have same origin code in a single S19 file (see ORG)

* Fossil SCM, and custom directory root markers for fully portable installations of project source code (see -I option and ?f and ?a placeholders)

* Improved listing display

Outcomes