Hi, I've managed to install and run KDS with USBDM and configure it successfully. I'm running a Ubuntu Server installation.
However, when I try to run (or debug) an application, there's an error in the final launch sequence:
Error in final launch sequence
Failed to execute MI command:
monitor reset halt
Error message from debugger back end:
"monitor" command not supported by this target.
Failed to execute MI command:
monitor reset halt
Error message from debugger back end:
"monitor" command not supported by this target.
"monitor" command not supported by this target.
I have GDB installed on KDS.
What could it be?
Thanks.
In my case I get that all the time when I have too many breakpoints enabled. Using KE06 chips that is two, and since you need 1 for main . . . I also get it if one of the breakpoints is not able to be properly set.
Hi Gustavo leal,
Could you tell me the full name of you chip?
What the detail operation system you are using? You can try it in windows 7 system, it can works ok.
You should make sure your USBDM can works in your platform.
About the configuration, you can refer to this link and check it again:
USBDM Functions in Eclipse (including Kinetis Design Studio)
Regards,
Jingjing
Hi. I'm using the MKL26Z64.
I'm running it on a Ubuntu 14.04 server with XFCE.
I managed to partially solve the problem.
One of the libraries required to launch the USBDM ARM GDB Server (libwx_gtk2u-unnoficial) was missing. I installed this library and tcl-8.5 and the GDB server launched.
Now I can flash the chip using the ARM Flash Programmer application, but I still can't do it from inside KDS.
Thanks,
Gustavo.
Hi Gustavo Leal,
From the kds_user_guide.pdf, it need ubuntu14.04 LTS,
So, maybe KDS in your ubuntu 14.04 with XFCE will have problem, you should better working in the operation system which KDS defined.
At least, when I working in Window7 ,USBDM can works ok.
Regards,
Jingjing