Hi, I have a problem in the installation of codewarrior 10.6, you can not install a driver and I get error code 0x80000000 . finishes installing
but processor expert not working properly. I install it in an environment of win 8.1 in a notebook .
What could be the problem ?
from already thank you very much
If Eclipse CodeWarrior usage on Windows Vista, Windows 7 or Windows 8, Administrator rights are required to install CodeWarrior, since the installer copies files into the System folder.
Your project workspace needs to be setup in any folder that you can fully access.
Fiona Kuang
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------