I am trying to setup a shared folder from a i.MX6 device and mounting it to a i.MX28 device, but it just ends up with the following error:
Server/Host:(i,MX6) Client:(i.MX28)
mount: RPC: Unable to receive; errno = Connection reset by peer
mount: mounting 192.168.0.140:/mnt/nfs on /mnt/nfsshare failed: Bad file descriptor
This is the mount command that I use
mount -t nfs 192.168.0.140:/mnt/nfs /mnt/nfsshare
I even tried, testing it by mounting it on the same board. I get the same error.
Commands [exportfs] and [showmount] show that it seems to work well.
Also below is the [/etc/exports] file content
/mnt/nfs 192.168.0.130(rw,sync,no_root_squash,no_subtree_check)
/mnt/nfs 127.0.0.1(rw,sync,no_root_squash,no_subtree_check)
NFS related Kernel config file look like below:
CONFIG_NETWORK_FILESYSTEMS=y
CONFIG_NFS_FS=y
CONFIG_NFS_V2=y
CONFIG_NFS_V3=y
# CONFIG_NFS_V3_ACL is not set
# CONFIG_NFS_V4 is not set
# CONFIG_NFS_SWAP is not set
CONFIG_ROOT_NFS=y
# CONFIG_NFSD is not set
CONFIG_NFS_USE_KERNEL_DNS=y
CONFIG_NFSD=y
CONFIG_NFSD_V2_ACL=y
CONFIG_NFSD_V3=y
CONFIG_LOCKD=y
CONFIG_LOCKD_V4=y
CONFIG_NFS_ACL_SUPPORT=y
CONFIG_NFS_COMMON=y
Any idea as to what is causing this error?
Am I missing any other configurations?
Best Regards
Yuri
It seems NFS server is unreachable from the client side.
Please make sure that your client (192.168.0.130) is able
to connect nfs server (192.168.0.140) via UDP
and NFS port is not disabled with firewall configuration.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Can you run "ping" successfully?
For additional information I run the following commands:
root@imx6q-myboard:~# rpcinfo
program version netid address service owner
100000 4 local /var/run/rpcbind.sock portmapper superuser
100000 3 local /var/run/rpcbind.sock portmapper superuser
100003 3 tcp 0.0.0.0.8.1 nfs superuser
100003 4 tcp 0.0.0.0.8.1 nfs superuser
100227 3 tcp 0.0.0.0.8.1 - superuser
100003 3 udp 0.0.0.0.8.1 nfs superuser
100003 4 udp 0.0.0.0.8.1 nfs superuser
100227 3 udp 0.0.0.0.8.1 - superuser
100021 1 udp 0.0.0.0.223.130 nlockmgr superuser
100021 3 udp 0.0.0.0.223.130 nlockmgr superuser
100021 4 udp 0.0.0.0.223.130 nlockmgr superuser
100021 1 tcp 0.0.0.0.190.156 nlockmgr superuser
100021 3 tcp 0.0.0.0.190.156 nlockmgr superuser
100021 4 tcp 0.0.0.0.190.156 nlockmgr superuser
root@imx6q-myboard:~# rpcinfo -p
No remote programs registered.
root@imx6q-myboard:~# rpcinfo -p 192.168.0.140
program vers proto port service
100000 2 tcp 111 portmapper
100024 1 udp 35734 status
100024 1 tcp 42242 status
100005 1 udp 37386 mountd
100005 1 tcp 55494 mountd
100005 2 udp 37386 mountd
100005 2 tcp 55494 mountd
100005 3 udp 37386 mountd
100005 3 tcp 55494 mountd
root@imx6q-myboard:~# rpc
rpc.idmapd rpc.nfsd rpcbind rpcinfo
rpc.mountd rpc.statd rpcclient
Is there a problem with portmap configurations? The [-p] is suppose to display host program right? But It says nothing is registered.
It also seems the system does not have [rpc.portmap] although [usr/bin/portmap] is present, are they related?
Best Regards
Yuri
Could you try to add "-o nolock" as well. Take reference from this: http://wiki.openwrt.org/doc/howto/nfs.client
Hello
Is there some sort of firewall or port opening configuration that I missed?
Just tested with L3.10.53_1.1.0-GA release pre-built image for i.MX6QSDB board and the NFS mount is running. Could try and then cross check your setup.
HW: i.MX6QSDB board
SW: fsl-image-qt5-x11-imx6qdlsolo.sdcard
Host Linux PC: Ubuntu 14.04 64bit OS with nfs packages installed:
$ sudo apt-get install nfs-common nfs-kernel-server
and added this to the /etc/exports:
/home/vmuser/ltib_src *(rw,no_root_squash)
Then, power up the i.MX6QSDB board with SD card programmed with the fsl-image-qt5-x11-imx6dqdlsolo.scard and then type the follows:
# mount -t nfs -o nolock 10.192.246.82:/home/vmuser/ltib_src/gpu-sdk /mnt
# mount
:
:
10.192.246.82:/home/vmuser/ltib_src/gpu-sdk on /mnt type nfs4 (rw,relatime,vers=4.0,rsize=524288,wsize=524288,namlen=255,hard,proto=tcp,port=0,timeo=600,retrans=2,sec=sys,clientaddr=10.192.246.85,local_lock=none,addr=10.192.246.82)
Thank you for looking into this. Sorry that I didn't make the setup clear.
Both the host(i.MX6) device and client(i.MX28) devices are i.MX devices.
I tried on both devices in mounting folders/file from a Host PC(Ubuntu 12.04) and there seem to be no errors.
The problem arises when the i.MX6 device is the server/host. I cannot connect from the i.MX28 device,
although the ping is fine and the i.MX28 device can [showmount] the shared folders from the i.MX6
Best Regards
Yuri
Hello
I have also tried those option with same results. Also tried specifying ports and proto.
One more thing, whenever I run the mount command and get the [Connection reset by peer] error, [showmount -e] does not display anything anymore.
I have to restart nfs on the server side for it to work again.. Is this normal behaviour?
(Btw, I have configured a samba server on the same device and the client device has no problem mounting and accessing the shared folder)
Hello,
Yes. And command [showmount] from the client lists the shared folders properly.
Only connecting to it seems to be the problem.
Best Regards
Yuri