AnsweredAssumed Answered

Synchronous Mode settings.

Question asked by Takashi Takahashi on Mar 18, 2015
Latest reply on Mar 30, 2015 by alejandrolozano

Dear community.

 

I refer Vybrid RM of Table 9-6. Synchronous Mode.

There are 4settings are described..

 

Is this the 4 settings example?

Do Will Do not the other settings?

 

I need to the connect to I2C rating of the destination will need to the IPG below 20MHz.

 

For example,Theparameter set is PLL1-> PFD3 (396MHz), ARM_DIV = 1, BUS_DIV = 5, IPG_DIV = 4 ,will be IPG = 19.8MHz

But this settings not stated in Table 9-6.

Do the above setting is possible?

For the use of there is no parameter set forth in Table 9-6, or there is no concern?

Outcomes