ALSA 5.1 Surround Sound with SSI/I2S on i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ALSA 5.1 Surround Sound with SSI/I2S on i.MX6

1,645 Views
joshkurland
Contributor IV

Hello,

I would like to know if it is possible to implement 6 channel, 5.1 Surround Sound audio playback by using three SSI ports.  Each SSI will carry one stereo audio pair to an I2S device.  In order to avoid errors, the three SSI ports must be synchronized with each other.  Is their a register mode that will achieve this?

Thank you,

Josh K.

Labels (3)
0 Kudos
1 Reply

648 Views
igorpadykov
NXP Employee
NXP Employee

Hi Josh

I think this is feasible, for synchronization one can use external frame signal.

Also it may be useful to look at attached i.MX6/35 Linux Manuals sect.23.2 SoC Sound Card

7.1 sound card, sect.7.1 SoC Sound Card for  5.1 sound card.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos