We are using ARM i.MX6U MCIMX6U7CVM08AC
What family does this chip fall under and which BSP do I need?
[ro.build.display.id]: [1.1.0-rc4]
[ro.build.fingerprint]: [Freescale/sabresd_6dq/sabresd_6dq:4.3/1.1.0-rc4/20131206:user/dev-keys]
[ro.build.host]: [madspeed]
[ro.build.id]: [1.1.0-rc4]
[ro.build.product]: [sabresd_6dq]
[ro.build.tags]: [dev-keys]
[ro.build.type]: [user]
[ro.build.user]: [b18293]
[ro.build.version.codename]: [REL]
[ro.build.version.incremental]: [20131206]
[ro.build.version.release]: [4.3]
[ro.build.version.sdk]: [18]
Hello Desiree,
It is a dual processor, so you should use the i.mx6DQ
List of BSPs is here:
SABRE for Smart Devices Reference Design|Freescale
Under "run-time software"
Have a great day,
Sergio
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------