Thanx, for your kind reply. I observed a strange problem.
From last two days I want to run the example for HCS12DP256B give at following path C:\Program Files\Freescale\CW for HC12 V4.5\(CodeWarrior_Examples)\MC9S12\DP\DP256B.
C:\Program Files\Freescale\CW for HC12 V4.5\(CodeWarrior_Examples)\MC9S12\DP\DP256B.
Due to that reason I connected a null modem RS-232 cable to M68KIT912DP256 to see serial output . After that I performed steps as follow.
1) Install the Multilink driver that was download from www.pemicro.com. I am using WINXP and Multilink device was not shown in the device manager.
2) Check the entire jumper setting that was same as u wrote in your mail.
3) Then connect USB MULTILINK to the PC the Multilink blue LED became ON.
4) Then I powered up the KIT. Multilink Yellow LED become ONand Bargraph on the Kit was glowing.
5) Run the Real-Time Simulator and debugger by click on the Icon of DEBUG. But no connection was made.
After it I disconnect all cables and then again make all connections but RS-232 cable did not attach. But this time only blue light was ON though Kit was powered then I connect the RS232 cable with Powered KIT then Yellow light became ON.
I repeat this process many times again but
I conclude that may be there was a unknown wrong jumper setting or Multilink is not functioning proper or winxp driver is not recognizing the Multilink
Please guide me soon because I have to complete given task with finite time.