S12ZVM boost converter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12ZVM boost converter

Jump to solution
547 Views
ikkishingu
Contributor II


Hello,

 

Please check whether my understanding is correct about S12ZVM boost converter.

 

There are the specs about boost converter in S12ZVM as below,

VSUP boost turn on trip point V_BSTON : min 9.5V, typ 10.1V, max 10.6V

VSUP boost turn off trip point V_BSTOFF : min 9.75V, typ 10.3V, max 10.8V

My understanding is that:

--

1. These means

- when the VSUP becomes below V_BSTON, then the boost converter operates

and

- when the VSUP becomes above V_BSTOFF, then the boost converter doesn't operate.

 

2. Therefore, there is the hysteresis features and the boosted VSUP voltage has a ripple equivalent to V_BSTON-V_BSTOFF during boosting.

--

 

Is my understanding correct?

 

Best Regards,

Ikki

Labels (1)
Tags (1)
0 Kudos
1 Solution
393 Views
iggi
NXP Employee
NXP Employee

Hi,

Well, yes, your understanding is correct. In case of low voltage on VSUP pin the boost converter operates (assuming that GBOE bit is set).

Not sure about the ripple. There are two capacitors in the external circuit of the boost converter. So the ripple should be reduced.

Regards,

iggi

View solution in original post

0 Kudos
2 Replies
394 Views
iggi
NXP Employee
NXP Employee

Hi,

Well, yes, your understanding is correct. In case of low voltage on VSUP pin the boost converter operates (assuming that GBOE bit is set).

Not sure about the ripple. There are two capacitors in the external circuit of the boost converter. So the ripple should be reduced.

Regards,

iggi

0 Kudos
393 Views
ikkishingu
Contributor II

Dear iggi,

Thank you for your information!

ikki

0 Kudos