Hi
We use MX6QDL_PAD_EIM_D28 as our spi4 MOSI, but we can't ecognized SPI flash
And we use oscilloscope to measure EIM_D28,we found a strange phenomenon
As shown in below
At boot time, host will send deivce id(0X9F) to SPI,but before sending device id, EIM_D28 have a pulled LOW signals.
It will make the host sends the id becomes 0x1f.
We also have another SPI5,it will not have the phenomenon.
Both of them,we set pin control as below in dts file
MX6QDL_PAD_EIM_D28__ECSPI4_MOSI 0x170f1
MX6QDL_PAD_SD1_CMD__ECSPI5_MOSI 0x170f1
Please help to investigate this issue.
Thanks.
Hi,
Have you checked that that pin MX6QDL_PAD_EIM_D28__ECSPI4_MOS is not used in any onther node?
If it is used I recommend you to disable the module that is using it.
Best Regards,
Alejandro
Hi
We don't use this pin for the other modules
And I try to send two message ,but I found that there were still a low signals before send each message,
As shown in below
Are there any usage restrictions on the pin?
Thanks.