I need to enable CONFIG_SYS_POST_UART & CONFIG_SYS_POST_ETHER for t1040rdb in u-boot as I'm not sure it is enabled by default in u-boot.
For the same I have provided following in "inclue/configs/T104xRDB.h"
#define CONFIG_POST (CONFIG_SYS_POST_UART | CONFIG_SYS_POST_ETHER)
Now I could see POST for UART is trace-down to uart_post_test() of "./drivers/serial/serial.c" but couldn't trace same POST for ETHER.
Though ether_post_test() is defined in "./post/cpu/mpc8xx/ether.c" but I don't see ether.c is getting compiled ?
So, What I need to do to enable CONFIG_SYS_POST_UART & CONFIG_SYS_POST_ETHER properly?
Thanks,
Amit
Look at the u-boot readme file using the following page:
http://git.denx.de/?p=u-boot.git;a=blob_plain;f=README;hb=HEAD
Find the Section “Configuration Options:” in this file.
This Section contains the following:
Configuration depends on the combination of board and CPU type; all such information is kept in a configuration file "include/configs/<board_name>.h".