please help about bus clock of S12ZVMC12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

please help about bus clock of S12ZVMC12

424 Views
Fan_xy
Contributor III

Hello all,

 

I have ask a question about the bus clock of S12ZVMC12 ,

Please see here : How to cacluate the bus clock of S12ZVMC12

I use CW 10.6 , create PE project .

When i use "Internal clock" , it is 1MHZ, what's the biggest bus clock ?

 

When i select  30MHZ or 50 MHZ "Internal bus clock " , when build , there is no error ,while , when debug , it show

 

20640_20640.pngpastedImage_0.png

 

 

Could you tell me what's wrong with me .

And when i select 20 MHZ bus clock , it can work well .

 

 

Thank !

Labels (1)
0 Kudos
1 Reply

253 Views
iggi
NXP Employee
NXP Employee

I don't understand why you opened a new topic when there is the same question in the existing one:

How to cacluate the bus clock of S12ZVMC12

0 Kudos