Kinetis KL03 VDDA pin?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis KL03 VDDA pin?

Jump to solution
619 Views
adriengambino
NXP Employee
NXP Employee

In the Kinetis KL03 datasheet, i don't see a pin for VDDA, only for VDD. Is VDDA internally connected to VDD? Thanks.

Labels (1)
0 Kudos
1 Solution
457 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Adrien:

That is correct, VDDA is internally connected to VDD when not available externally. This is from KL03 Reference Manual:

pastedImage_1.png

Regards!,
Jorge Gonzalez
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
458 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Adrien:

That is correct, VDDA is internally connected to VDD when not available externally. This is from KL03 Reference Manual:

pastedImage_1.png

Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos