Hello Champs,
i.MX50 can connect 16bit DDR2 but there is description how to connect 16 bit DDR2 x 1.
Is it possble to connect 16 bit DDR2 x 1 as a following diagram?
Please see numbers in Red.
In the SDG, there is a Vref resistor size table as follows
What is the size in case DDR2 1pcs?
Best regards,
Nori Shinozaki
Hi Nori
right, such connection can be used and
resistors can be 1K 1% as implemented on i.MX28 EVK
and suggests Micron tn4614.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Igor,
Thanks!
Nori Shinozaki