How to set i.MX6 EIM_BOOT_CFG bus?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to set i.MX6 EIM_BOOT_CFG bus?

Jump to solution
740 Views
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6SDL EIM boot.

Please see chapter 6.4.3 in IMX6SDLRM Rev.1.

It shows EIM_BOOT_CFG bus, but we did not understand what is this because this config bus is not mentioned in chapter 8 "System Boot".

Would you let me know how set EIM_BOOT_CFG bus?

Best Regards,

Satoshi Shimoda

Labels (4)
Tags (2)
0 Kudos
1 Solution
600 Views
Yuri
NXP Employee
NXP Employee

"EIM_BOOT_CFG bus" is internal bus, from it only MUM signals

are routed externally according to Table 8-9 "EIM Boot eFUSE Descriptions".

Other signals are fixed internally and can not be changed at boot.

You can ignore it, it is not used for boot from EIM. Please use only Table 8-9


Have a great day,
Yuri
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
601 Views
Yuri
NXP Employee
NXP Employee

"EIM_BOOT_CFG bus" is internal bus, from it only MUM signals

are routed externally according to Table 8-9 "EIM Boot eFUSE Descriptions".

Other signals are fixed internally and can not be changed at boot.

You can ignore it, it is not used for boot from EIM. Please use only Table 8-9


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos