Hi,
After running ./mxc_v4l2_overlay.out no display is visible on screen. Ideally adv7180 data should be overlayed on ubuntu desktop.
I get following errors:
ERROR: v4l2 capture: slave not found! |
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
And after running gst-launch tvsrc ! mfw_v4lsink,
I get following errors:
Internal data flow error
streaming task paused, reason error (-5)
Still no display on HDMI as well as VGA.
Can anybody help ???? i am on a very tight timeline.
Solved! Go to Solution.
I got it. It was a hardware problem. The adv7180 was connected to arm and as an option to the FPGA. The FPGA pins were not configured in input mode.
I got it. It was a hardware problem. The adv7180 was connected to arm and as an option to the FPGA. The FPGA pins were not configured in input mode.