Unable to connect the JTAG to i.MX6 Quad processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to connect the JTAG to i.MX6 Quad processor

1,073 Views
muralikrishna
Contributor I

We are using i.MX6 Quad Processor in our design.  The boards are fabricated with i.MX6 processor. In the new boards we are unable to connect the J-Link JTAG (Segger). When we connect J-link JTAG, it is dipalying as message that Device is not connected at all" and it is not diplaying device id also.

For new processors is we need to program first anything before JTAG communication. Kindly clarify.

Labels (1)
0 Kudos
1 Reply

523 Views
Yuri
NXP Employee
NXP Employee

Please check Your design regarding Design Checklist recommendations in Chapter 2

(Design Checklist) of IMX6DQ6SDLHDG : Hardware Development Guide for i.MX 6Quad,

6Dual, 6DualLite, 6Solo Families

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Please pay attention on Table 2-5 (JTAG recommendations).

Also, the following may be useful :

Re: Debugging U-boot on iMX6

Re: J-Link and iMX6


Have a great day,
Yuri.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos