Hello,
I have successfully configured and installed LTIB.
uImage, kernel and filesystem have been created.
Now i transferred uImage and kernel on SD-Card, when i started the board, it shows following.
=====================================================================================
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: ncq stag pm led clo only pmp pio slum part
No port device detected!
** Bad device size - sata 0 **
** Bad device size - sata 0 **
SATA device 1: unknown device
** Bad device sata 1 **
** Bad device sata 1 **
MMC: no card present
mmc0(part 0) is current device
MMC: no card present
** Bad device mmc 0 **
MMC: no card present
** Bad device mmc 0 **
mmc1 is current device
** Unrecognized filesystem type **
Failed to mount ext2 filesystem...
** Unrecognized filesystem type **
(Re)start USB...
USB0: lowlevel init failed
USB1: USB EHCI 1.00
scanning bus 1 for devices... 2 USB Device(s) found
scanning usb for storage devices... 0 Storage Device(s) found
scanning usb for ethernet devices... 0 Ethernet Device(s) found
USB device 0: unknown device
** Bad device usb 0 **
** Bad device usb 0 **
USB device 1: unknown device
** Bad device usb 1 **
** Bad device usb 1 **
6x_bootscript not found
serial console at 115200, 8N1
details at http://boundarydevices.com/6q_bootscript
========================================================================================
Can anyone please tell me what the problem is? How should i transfer the images? Or Any configuration I am missing?
Hello Hitesh,
I'm not familiar with the sabre lite, but I'm attaching our Linux user guide, which explains how to copy your files to the SD card in chapter 8, copying to the SD card should be exactly the same.
Have a great day,
Sergio
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks SergioSolis,
I would go through these step, but i have corrupted my SD-Card.
I would love to format SD-Card from the start, Can you please tell me what steps or partition should have, for the same. As formatting or partition info is not given there.
You can use FDisk to erase all partitions and create them according to the linux user guide.