AnsweredAssumed Answered

K60 controller adc programming

Question asked by Lijo Francis on Feb 25, 2015
Latest reply on Feb 26, 2015 by Drew Kelley

dear sir,

i dont understand adc configuration in k60.i read there is ADC0,ADC1,ADC2,ADC3,

and there is adcx_se*a and adcx_dm0,adcx_dp0

i dont understand it.

 

how many channel can we connect at the same time that is how many analog inputs can we connect

which pins are used for analog input

what the analog pins used for

differential analog inputs ,which are two analog inputs

how can we use dma,

dma used it automatically convert the channel we specified at the memory location

 

please tell me

please sir dont reply with k60 datasheet that i have,

is there is any simple functional circuit

Outcomes