AnsweredAssumed Answered

SD card boot failed(only build image)

Question asked by kong king on Feb 23, 2015
Latest reply on Feb 27, 2015 by kong king

hello community.

 

 

 

I have a i.MX6Q sabre lite. And host setting is Ubuntu 14.04.2 LTS 64bit.

 

 

 

https://github.com/Freescale/fsl-community-bsp-platform

 

(I visited this web site.)

 

 

 

Referred to 'FSL Community BSP' tab

 

 

 

+add

 

 

 

$: vi conf/local.conf

 

 

MACHINE           = "imx6qsabrelite"

 

 

$ cd tmp/deploy/images/imx6qsabrelite

 

 

(Occurred imx6q sabrelite directory. so I Took action.)

 

 

I connected the SDcard to the host pc

 

 

and try this.

 

lite@emb:~/fsl-community-bsp/build/tmp/deploy/images/imx6qsabrelite$ sudo dd if=core-image-minimal-imx6qsabrelite.sdcard of=/dev/sdc1

49152+0 records in

49152+0 records out

25165824 bytes (25 MB) copied, 3.84026 s, 6.6 MB/s

 

 

 

 

 

but...

 

 

 

 

lite@emb:~/fsl-community-bsp/build/tmp/deploy/images$ df -h

Filesystem      Size  Used Avail Use% Mounted on

/dev/sda1       226G   23G  192G  11% /

none            4.0K     0  4.0K   0% /sys/fs/cgroup

udev            1.9G  4.0K  1.9G   1% /dev

tmpfs           382M  1.2M  381M   1% /run

none            5.0M     0  5.0M   0% /run/lock

none            1.9G  492K  1.9G   1% /run/shm

none            100M   60K  100M   1% /run/user

/dev/sdc1       7.4G  4.0K 7.4G   1% /media/lite/0AD3-D456

 

 

and Do not host PC connect.

 

 

 

 

 

 

 

I'm retry.

 

 

 

(copy&paste the core-image-minimal-imx6qsabrelite.sdcard file.)

 

lite@emb:~/fsl-community-bsp/build/tmp/deploy/images/$ sudo dd if=core-image-minimal-imx6qsabrelite.sdcard of=/dev/sdc1

 

 

However, the result is the same as that of the front.

 

 

 

 

 

 

 

And boot failed... perfect failed..

 

 

 

 

 

 

 

 

 

thanks for reading.

 

 

 

please help!

Outcomes