Pascal Irrle

Re: what i do if i want to make high only one pin of any port of MC9S12XDP512//Please Somebody give me answer

Discussion created by Pascal Irrle Employee on Feb 20, 2015
Latest reply on Feb 24, 2015 by Pascal Irrle
Branched from an earlier discussion

Hi,

 

May be there is some example delivered with the board if a DVD was included in the pack.

Else you can find some example of Freescale web site.

 

CodeWarrior for Hc12 v5.1 is the last version.

It integrates Processor Expert (Code Generator) which help you to create, configure all peripherals.

Several examples are delivered on the installation with and without processor Expert.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

Outcomes