HABv4.1 vs. TPM1.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HABv4.1 vs. TPM1.2

Jump to solution
1,786 Views
TMain
Contributor III

I was wondering how the HABv4.1 function of the Security Engine in the iMX6 compares to the TPM1.2 (Trusted Platform Module) standard. Does implementing the HAB functionality of the iMX6 meet the TPM1.2 standard?

0 Kudos
1 Solution
938 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
2 Replies
939 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
939 Views
Yuri
NXP Employee
NXP Employee

  Strictly speaking, the HAB technology is not intended to meet the TPM1.2.

High Assurance Boot (HAB) is just Freescale’s implementation for secure boot. 


Have a great day,
Yuri.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos