eMMC 5.0 Support for i.Mx6 Processors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eMMC 5.0 Support for i.Mx6 Processors

2,150 Views
pankajrana
Contributor III

Hi,

Does the i.Mx6 SoloLite processor support "e.MMC 5.0 with HS400 Interface" ?

After studying few posts in the community, I could not arrive to a conclusion:

Re: i.mx6 with eMMC 5.0 SDR or DDR interface?

Does i.MX6 quad core processor support eMMC 5.0 HS400 interface

Let me know your comments on this.

Thanks.

Regards,

Pankaj Rana

Labels (1)
Tags (4)
0 Kudos
5 Replies

930 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pankaj

no, HS400 is not supported.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

930 Views
pankajrana
Contributor III

Dear Igor,

For your above mentioned comments:

"Hi Pankaj

no, HS400 is not supported.

Best regards

igor"

Now, not considering the HS400, will the SoloLite Processor support eMMC 5.0 ?

Regards,

Pankaj Rana

0 Kudos

930 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pankaj

not, according to IMX6SLRM sect.54.1.1 Features

..

• Compatible with the MMC System Specification version 4.2/4.3/4.4/4.41

Best regards

igor

0 Kudos

930 Views
pankajrana
Contributor III

Hi Igor,

Few clarifications on eMMC interfacing with SoloLite Processor:

iMX6SLRM

Chapter 5: Fusemap

Table 5-5. MMC/eMMC Boot Fusemap

0x450[15:8]                    Port Select:

(BOOT_CFG2)               00 - uSDHC1

                                     01 - uSDHC2

                                   10 - uSDHC3 (eMMC4.4)

                                     11 - uSDHC4

Does that mean that eMMC4.4 is supported only on uSDHC3 ?

Whereas in Chapter 8:System Boot , section 8.5.2.1 , it is mentioned "All USDHC ports support eMMC4.3 and eMMC4.4 fast boot."

Also in Table 8-15. :

eMMC Reset Enable    -    "eMMC reset enabled via SD_RST pad (on USDHC3 and USDHC4 only)"

Please clarify this, at the moment there is uncertainty regarding the eMMC usage and USDHC port selection.

Many Thanks.

--Pankaj Rana

0 Kudos

930 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pankaj

All USDHC ports support eMMC4.3 and eMMC4.4.

~igor

0 Kudos