AnsweredAssumed Answered

PEx SPI Bidirectional mode

Question asked by Juanma Bailen on Feb 20, 2015
Latest reply on Mar 27, 2015 by Juanma Bailen

Hi people

 

Previously I used the S08 microntroller and the SPI Processor Expert component allowed me to used the "Bidirectional mode" (see attached file 01.png). The description says this option is only available for Coldfire, S08 and S12.

 

Nowadays I'm working with the MKE02Z64 microntroller and the PEx doesn't let me to choose the setting Bidirectional mode, but in the datasheet says that it's an option you can set (02.png > KE02 Sub-Family Reference Manual > 29.4.6.2 Bidirectional mode (MOMI or SISO) page 513).

 

Do I need to configure it manually?

 

Thanks!

Attachments

Outcomes