how to flash/debug using KL05Z+JLINK+KDS 2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to flash/debug using KL05Z+JLINK+KDS 2.0

Jump to solution
995 Views
gschelotto
Contributor V

Hello,

 

I'd like to flash/debug a KL05Z device using 5 pin (GND, 3V3, DIO, CLK, RST) with J-LINK Base and Kinetis Design Studio v2.0. Could anybody help me?

 

Thanks in advance,

gaston

Labels (1)
Tags (1)
1 Solution
607 Views
BlackNight
NXP Employee
NXP Employee
5 Replies
607 Views
santiago_gonzal
NXP Employee
NXP Employee

Hello Gaston,

What is your issue?

- How to do the hardware connection of the pins?

- How to create the debug configuration in KDS?

- How to create a project to flash inside the KL05 using KDS?

Regards,

Santiago

0 Kudos
607 Views
gschelotto
Contributor V

Hello Santiago,

Sorry for not being so clear.

Here's my current HW configuration

Untitled.png

So the question is related to how to create the debug configuration in KDS 2.0 with J-LINK.

regards,

gaston

0 Kudos
608 Views
BlackNight
NXP Employee
NXP Employee

Hi gaston,

have a read here: https://community.freescale.com/docs/DOC-101845

Erich

607 Views
gschelotto
Contributor V

Hi Erich,

I've followed the steps for the Segger J-LINK configuration but I get the next error

Untitled.png

I've also checked the trouble shooting tips but I'm still not able to start a debug session. Any hints?

regards,

gaston

0 Kudos
607 Views
gschelotto
Contributor V

Solved! I forgot to set GDB executable path correctly.

regards,

gaston

0 Kudos