AnsweredAssumed Answered

i.MX6 DRAM_SDCKEx external resistor.

Question asked by Satoshi Shimoda on Feb 16, 2015
Latest reply on Feb 27, 2015 by Satoshi Shimoda

Hi community,

 

I have a question about i.MX6SDL, i.MX6DQ DDR design.

Please see No.4 of Table 1-1 in IMX6DQ6SDLHDG "Rev.0".

It says "DRAM_SDCKE0 and DRAM_SDCKE1 should be connected to individual 10 kΩ5% resistors to GND."

On the other hand, No.4 of Table 2-1 in IMX6DQ6SDLHDG "Rev.1", It says "DRAM_SDCKE0 and DRAM_SDCKE1 no longer require external 10 kΩresistors to GND to minimize current drain during deep sleep mode (DSM)."

 

In fact, I got a following reply in past in SR# 1-1132121434.

=====

Internal pull down resistor of 100 KOhm provides relatively “weak” pulling down.

=====

 

Why the recommended disign was changed?

This weak pull down issue have been fixed?

 

 

Best Regards,

Satoshi Shimoda

Outcomes