Hi,
I'm trying the various ethernet-related examples of the KSDK 1.1 (lwip_ping_demo, lwip_httpserver_demo; I tried the bm and rtos code for the armgcc toolchain) on FRDM-K64F; no success, cannot connect/ping to the board, no output on the serial
after a bit of debugging I concluded that the ENET RX interrupt hander is not called, but why?
similar examples on mbed work OK for my board
is the example code supposed to work?
thanks, p.
Solved! Go to Solution.
Hi,
I tested the code lwip_ping_demo and configured the IP address according to the information of the Kinetis SDK v.1.1 API Reference Manual Chapter 16 and it runs without problems.
Here is a picture that shows the demo running:
You mentioned you have no output on the serial, that means you cannot see anything in the COMx port connected to the FRDM-K64F SDA connector? I recommend to run a simple Hello_World demo to ensure the Serial port is working correctly.
Hope this information can help you
Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Peter
You can also check out the following for FRDM-K64F and Ethernet:
http://www.utasker.com/kinetis/FRDM-K64F.html
It works out-of-the-box with KDS and also allows a second Ethernet port to be connected via SPI, based on the ENC424J600
Regards
Mark
Kinetis: http://www.utasker.com/kinetis.html
K64: http://www.utasker.com/kinetis/FRDM-K64F.html / http://www.utasker.com/kinetis/TWR-K64F120M.html
For the complete "out-of-the-box" Kinetis experience and faster time to market
Hi,
I tested the code lwip_ping_demo and configured the IP address according to the information of the Kinetis SDK v.1.1 API Reference Manual Chapter 16 and it runs without problems.
Here is a picture that shows the demo running:
You mentioned you have no output on the serial, that means you cannot see anything in the COMx port connected to the FRDM-K64F SDA connector? I recommend to run a simple Hello_World demo to ensure the Serial port is working correctly.
Hope this information can help you
Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
thanks for the confirmation; I got the examples working (most of the time at least)
the green LED on the FRDM-K64F RJ45 did not come up in one of the tries, not sure what is to blame
I cannot reproduce the issue anymore
regards, p.